12/1/2023 11:13 AM | |
Joined: 8/29/2023 Last visit: 5/13/2024 Posts: 3 Rating:
|
Good morning, I would like to know if there is any way to easily connect and communicate with a PLC s7-1500 using python. For this project, I am required to communicate to the PLC using PROFINET. NOTE: I am using TIA portal v16 and PLC Sim advanced V4. I do not have any physical hardware. I know that the python-snap7 library allows to read and write to and from a data block, but I'm still confused: does it uses PROFINET? Is it something else? Is PUT/GET violating the protocol? I am getting mixed information about snap7 and PROFINET. Sometimes PROFINET is mentioned, and the two things seem connected, other times it seems that they are not related. For reference, I'm looking for something like what is shown in this tutorial: https://www.solisplc.com/tutorials/introduction-to-snap7-integration-into-siemens-tia-portal, which I have no issue to replicate. Thank you in advanced for anyone that will help me. |
12/3/2023 9:55 AM | |
Joined: 5/22/2023 Last visit: 9/9/2024 Posts: 22 Rating:
|
I forgot the second image... sorry |
Follow us on