6/28/2011 1:35 PM | |
Joined: 2/23/2007 Last visit: 2/19/2023 Posts: 75 Rating: (1) |
Hi everybody, I am need write many strings on many DB,s. I am use a Siemens example:https://support.automation.siemens.com/WW/llisapi.dll?query=string&func=cslib.cssearch&content=adsearch%2Fadsearch.aspx&lang=en&siteid=cseus&objaction=cssearch&searchinprim=&nodeid99=&x=30&y=6 But when I change de block, I lost values and need write wich DB to correct name. Please see in the image! Thanks for any help. And sorry for my bad english. |
6/28/2011 1:44 PM | |
Joined: 1/28/2009 Last visit: 4/26/2024 Posts: 6838 Rating: (1359) |
Provide more information here to help us to undrestand your problem.At least upload your codes and restate the problem you find this solution for that.If you provide sufficient information here, members would suggest solution much easier. Regards |
Last edited by: hdhosseini at: 6/28/2011 1:45 PM |
|
This contribution was helpful to1 thankful Users |
6/28/2011 7:36 PM | |
Joined: 2/23/2007 Last visit: 2/19/2023 Posts: 75 Rating: (1) |
I want a function to write a string of one DB to other DB! But in screen not function. Thank for help!
|
6/29/2011 12:59 PM | |
Joined: 10/7/2005 Last visit: 4/28/2024 Posts: 3004 Rating: (1046)
|
Keep it simple guys if NewTechwants toonly copy a String from one DB to another, all he has tois use SFC 20 "BLKMOV" and assign the correct parameters. In NewTechexample screendump, the soruce String is in DB126,starts at Byte address 18 and is 18 Bytes long (16 characters plus 2 bytes header). Using "DB126.DBB50" for theSCRBLK parameter of SFC 20 as shown in hisscreendump is obviously wrong, butusing P#DB126.DBX18.0 BYTE 18 will work (or he uses symbolic declaration right away which is "DB_name".String_name). The same needs to be done for the DSTBLK parameter of SFC 20, but this is where NewTech'sexamplestarst to confuse me sincethe destination is the Instance DB location of an IN Parameter of an FB, so I'm really not too sure what exactly he wants to do (why not simply assign the source string to the call of the FB?). |
Cheers |
|
This contribution was helpful to1 thankful Users |
Follow us on