12/12/2017 1:34 PM | |
Joined: 8/3/2009 Last visit: 10/14/2024 Posts: 13919 Rating: (1757)
|
Hello jmlai there is a limitation that you can only store less than 256 files in the root path of an SD Card or USB Stick. But if you create own folders there is no limitation. Also there is no reachable limitation in writing lines to a Text or csv File. You can use this FAQ as template: https://support.industry.siemens.com/cs/ww/en/view/59604194 The only thing is to be sure that the script is finished before the next cycle starts. so 10 seconds it should be possible but if you want to write every 500ms I would not reccomend. Bye Murof |
If this Information really helps, you could use the Rate function |
|
Follow us on