4/6/2020 9:36 AM | |
Joined: 5/12/2006 Last visit: 7/11/2024 Posts: 22308 Rating:
|
Hello, yes this should be possible with S7 Routing. Regards Christoph |
4/9/2020 2:37 PM | |
Joined: 8/3/2009 Last visit: 7/12/2024 Posts: 13284 Rating:
|
Hello If you want to download the HMI Project or do a S7 Communication connection then it works with almost all Versions: https://support.industry.siemens.com/cs/ww/en/view/90528617 If you want to do a genereal IP routing then this is only possible in TIA Portal V16 and new 2.8 FW Bye Murof |
If this Information really helps, you could use the Rate function |
|
Follow us on