Industry Online Support
Technical Forum
12/17/2008 7:16 PM | |
Joined: 4/6/2006 Last visit: 2/5/2024 Posts: 604 Rating:
|
Hello Lauret, yes it's possible to use MRP in the Scalance X204 IRT if that's your question. An RM is an Redundancy Manager. To get more information about the working of an Ring like HSR (High Speed Redundancy Ring) you can have a look at the movie in the link below. There is a very nice movie which describes the HSR. The HSR is a ring technology available on all managed Scalance switches (X200, X200 IRT, X300 and X400). It can manage 50 switches in a ring with a typical reconfiguration time from 300 ms. For MRP it's possible to have 50 devices (CP's, Switches) in a ring with a typical reconfiguration time from 200 ms. Demonstration System "Redundancy Mechanisms" in industrial networks with SCALANCE X More information about MRP configuration can be found in the Manual via the link below.It's mentioned in Chapter 2.4. There is completely described how it is configured and what devices are allowed inside a ring. Manual Scalance X200 |
Best regards, |
|
12/18/2008 9:24 AM | |
Joined: 4/6/2006 Last visit: 2/5/2024 Posts: 604 Rating:
|
Hello Lauret, No, I'm sorry v4.0 is not available. But here you can find v4.1 which is brand new. Download v4.1 |
Best regards, |
|
Follow us on