4/15/2022 6:30 AM | |
Joined: 8/24/2018 Last visit: 6/3/2024 Posts: 22 Rating: (0) |
Background I downloaded the getting started Siwarex CS project that has both the S7 classic project and HMI project. I modified the project to the HW that I have (CPU315-2PN/DP) and KTP1000 for the WinCC Flex project. The Step 7 project works I can get process value from the load cell and see it on my project. With the KTP1000 I was not able to download the project using the Profibus. I managed to download it using the USB-PPI (RS485 serial). Problem Now I have the projects running in all my HW however the HMI is still not communicating with the PLC. Also when I check accessible nodes, I cannot see the address of the HMI. Even if I unplug the profibus cable from the HMI, I don't get the bus fault. I have attached all the configuration settings: S7-HW Configuration WinCC Flex connection NetPro MPI/DP Settings of HMI AttachmentConfiguration.zip (445 Downloads) |
Automation is about making things talk |
|
4/15/2022 8:35 AM | |
Joined: 4/24/2006 Last visit: 7/9/2024 Posts: 8711 Rating: (1165) |
Hello, Can you check on the panel, the settings for Profibus? (Advanced settings) Best regards, Wizard |
Follow us on