11/11/2023 7:24 PM | |
Joined: 7/28/2021 Last visit: 6/21/2024 Posts: 1 Rating:
|
Hi I need support I have a process that is constantly stopping but the PLC is not going to stop. Only the machinery stops, the operator clears the alarms, starts the machine again and that's it until it stops again, this can happen 3 times in a day. The failures reflected in the diagnosis are: Area length error when reading 16#2522; FC62 not loaded. But the FC is in the program 16#2522 ... when an address is being used that is not completely within the possible address area. Example: MW 320 must be read although the memory area is only 256 bytes long. FC not loaded 16#253c; FC 62 AND FC 40 (ONLY FC62 IS IN THE PROGRAM) DB not loaded16#253A; DB17 (not in the program) FC 62 (if in the program) What could be happening? How can I solve this error? The PLC is S7-400 ------------------------------------------------------------------------------------------ |
Last edited by: Benitorhm at: 11/13/2023 01:40:57Last edited by: Jen_Moderator at: 11/13/2023 10:53:10New subject after splitting |
|
Follow us on