11/14/2024 10:53 AM | |
Joined: 5/27/2024 Last visit: 8/26/2025 Posts: 54 Rating:
|
Hi, Which Ethernet switch can I use for Modbus TCP communication in S7-1200 PLC? |
11/14/2024 11:58 AM | |
Joined: 7/10/2024 Last visit: 9/19/2025 Posts: 180 Rating:
|
Hello! For Modbus TCP communication in an S7-1200 PLC, you can use the CSM 1277 Industrial Ethernet switch. The CSM 1277 is designed specifically for the S7-1200, allowing you to connect the PLC and up to three additional devices to an Industrial Ethernet network. Here you can see the details. - COMPACT SWITCH MODULE CSM 1277 I hope it helps |
If you found this post helpul, I'd greatly appreciate your feedback with the rate function |
|
This contribution was helpful to
1 thankful Users |
Follow us on