6/30/2025 2:29 PM | |
Joined: 2/1/2010 Last visit: 9/15/2025 Posts: 213 Rating:
|
Its buried deep in the help files, the attached is copied from the "Block Icon Structure" in PUD. "Memo View" in PUD gives other relevant info about the file format requirements. AFAIK there is not a direct way for bulk editing since these are properties on the block icon. But, with significant editing of block icons and block properties anything is possible NoteView documents You can configure a maximum of three files per block symbol instance, which can be selected in the memo view during the process control and are displayed in a separate window. These files must be located in theGraCS folder in theNoteView subdirectory. The file names are configured at the block icon at the attributesNoteView1,NoteView2 andNoteView3. Only.mht file formats are supported and the file extension ".mht" must be given (for example, "File1.mht") at the configuration. Note
|
If my post helped you, please rate. Thanks. |
|
This contribution was helpful to
2 thankful Users |
Follow us on