8/6/2025 2:35 PM | |
Joined: 2/1/2010 Last visit: 9/15/2025 Posts: 212 Rating:
|
Officially we have to go by the published list, even tech support may give you some issues with support. Unofficially, it should work fine. However that controller has different performance limitations with new(er) versions of APL blocks and communications so caution should be exercised when using anything that is not an AS410 in combination with APL moving forward. If you have upgraded the APL version along with your project, then you should be checking the system performance before placing into operation and have contingency for alternate path. (rollback, replace with AS410, etc.) |
If my post helped you, please rate. Thanks. |
|
Follow us on