12/22/2005 2:47 PM | |
Joined: 10/19/2005 Last visit: 11/30/2020 Posts: 1611 Rating: (121) |
Hi Will, Perhaps this link will help you. => http://support.automation.siemens.com/WW/view/de/15263615 Merry christmas |
12/30/2005 1:34 PM | |
Posts: 23 Rating: (1) |
Indeed, this brought me to the idea that I should have looked at the Windows Scripting Host. At the page: http://msdn.microsoft.com/library/default.asp?url=/library/en-us/script56/html/f482c739-3cf9-4139-a6af-3bde299b8009.aspI found the 'Popup method'. I have put in an event calling the script as stated and then I have an integer giving me a result value on which action can be taken. Thinking further: It would be nice to not only have the available button types (0-5) but to configure these buttons. So not the text 'Yes' - 'No', but (for a manual command to a valve) 'Open' - 'Close'. Thank you for the merry christmas and wishing you a nice 2006. Wil |
Follow us on