10/18/2022 2:09 PM | |
Joined: 5/30/2022 Last visit: 4/25/2024 Posts: 520 Rating: (85) |
Hi OMKRIS2017, I think you will not have any problem, you can try to add some PLC of another brand to these projects to see if it works. Attachment2022-10-18 16_09_01-Library of Basic Processes (LBP) V2.7 for TIA Portal V17 (STEP 7 Basic _ Profess.png (534 Downloads) |
If this information really helps, you could use the Rate function. |
|
11/14/2022 1:45 PM | |
Joined: 6/23/2013 Last visit: 4/18/2024 Posts: 54 Rating: (3) |
WinCC OA comes with a wide range of drivers to use many different PLCs. I do not all protocols your PLCs can handle, but I guess Ethernet/IP and modbus are good candidates. For the webpages development I would look at the Dashboard functionality or if you prefer to build them from scratch the HTTP server. |
WinCC OA specialist |
|
This contribution was helpful to1 thankful Users |
Follow us on