2/17/2023 8:23 AM | |
Joined: 8/3/2009 Last visit: 4/26/2024 Posts: 12869 Rating: (1641)
|
Hallo if the login information when accessing a network drive from a panel comes again and again, then there is usually something wrong with the configuration or you are not using a special user. (that there is nothing in the dialog is normal when you open it again) https://support.industry.siemens.com/cs/ww/en/view/92346478 or do you work with WinCC flexible -> LINK Viele Grüße Murof |
If this Information really helps, you could use the Rate function |
|
Follow us on