2/6/2023 1:52 PM | |
Joined: 5/12/2006 Last visit: 9/18/2024 Posts: 22364 Rating: (3011)
|
switch from "show compatible devices" to "with same IP" and try it again |
2/6/2023 2:01 PM | |
Joined: 2/6/2023 Last visit: 2/7/2023 Posts: 2 Rating: (0) |
Same errors, does not display anything.
|
2/6/2023 2:19 PM | |
Joined: 7/9/2015 Last visit: 8/30/2024 Posts: 3943 Rating: (585)
|
Hi, it could be a problem with your interface driver ord with PLC. Can you try to download project directly to Memory Card? How do you create the project data for the SMC so that you can download the project to the S7-1200/S7-1500 CPU even without STEP 7 (TIA Portal)?Regards, Towome |
|
|
2/7/2023 12:12 AM | |
Joined: 10/7/2005 Last visit: 9/19/2024 Posts: 3021 Rating: (1054)
|
Had the same "Incompatible device detected at address x.y.z" recently with Portal V17(upd5) and a 1515-2 CPU. "Online and diagnostics" claimed to be able to go online, but the "Reset to factory settings" as well as "Format memory card" functions were grayed out and thus no good. Ended up taking the memory card out, putting it into a spare 1500 CPU (different type but that doesn't matter) and used the "Format memory card" functions there. Put memory card back into the real CPU which now had the "Reset to factory settings" as well as "Format memory card" functions available, did a factory reset to be sure to be sure, downloaded the Portal project again and was back in business. All up a bit of an ordinary experience to say the least, no firm clue what caused this to start with and there's probably other ways to fix it too (e.g. format via PG, use the display for resets/format if you have one and subject to protection level etc.) |
Cheers |
|
This contribution was helpful to2 thankful Users |
Follow us on