1/23/2022 8:23 PM | |
Joined: 1/26/2007 Last visit: 8/27/2024 Posts: 123 Rating: (4) |
Hello, Friday i have installed TIA V 17 along TIA V14 that i was using for long time, but yesterday i was seeing i am not able to use OPEN VPN anymore. For me , i was able to establish connection to target, but i was not able to open online connection=> BSOD. For me was strange cause after i was establish connection and ping target=> BSOD. First i have made the first solution and unclick SIMATIC Industrial Ethernet(ISO), but after this i was not able to ping target/ or connect. After install both of update from link everithing is ok. Thank you for help! |
This contribution was helpful to1 thankful Users |
4/7/2022 9:10 AM | |
Joined: 5/4/2020 Last visit: 6/13/2024 Posts: 1 Rating: (0) |
Yes it works. I was very frustate with it, if is necessary to work from home. Many thanks to U. |
6/9/2022 2:14 PM | |
Joined: 6/9/2017 Last visit: 6/27/2024 Posts: 6 Rating: (0) |
This fixed my problem with FortiClient VPN 7.0.5.0238 and TIA Software V15.1. Thanks! |
Follow us on