3/6/2023 11:57 PM | |
Joined: 5/1/2017 Last visit: 6/27/2024 Posts: 1 Rating: (0) |
I encountered same issues here. I'm using SINUMERIK 840D Powerline with 611D. Interestingly, I managed to get the things work for the first axis by monitoring the Load and the Current. But when I proceed with the axis 2 and axis 3 for monitoring their load, I got 0 values. Steps are the same as I did for the first axis. I have called FB2 two times inside FC70 which is being called in OB1. The reason is the first FB2 in FC70’s has been reserved for the first axis which is in this case I’m monitoring the load and the current and it is working fine. The second FB2 in FC70’s network is to monitor the other load parameters, e.g Z and X axis. After downloading all block to NCU, I got the 0 values for both second and third axis. Is there anything wrong when downloading the DB and FC to the NCU? Thank you. ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 03/07/2023 10:12:13New subject after splitting |
|
3/8/2023 3:56 AM | |
Joined: 4/23/2010 Last visit: 12/31/2023 Posts: 8092 Rating: (877)
|
Can you attach your FB & FC here? |
Follow us on