3/13/2023 1:33 AM | |
Joined: 1/10/2020 Last visit: 3/29/2024 Posts: 45 Rating: (0) |
Hi All, May i know how to get Esupport software that mention at below: ---------------------------------------------------- Replace PCU50 V1 by PCU50 V2 To do this, the software stored on the ”PCU50 V1” ´must be converted to ”PCU50 V2”. This requires the following steps:
This creates a basic PCU software WinNT 4.0 V07.02.01 on the PCU 50 V2 - with the same functions as V06.02.01, however, with the drivers required for ”PCU 50 V2”. On this basis, all HMI-Base 6.x and HMI-Advanced 6.x software versions released so far are still executable. ---------------------------------------------------------------------------------- Attachmentchange_76.pdf (289 Downloads) |
Follow us on