4/6/2021 6:12 AM | |
Joined: 5/12/2006 Last visit: 5/1/2024 Posts: 22243 Rating: (2981)
|
use a new empty project |
This contribution was helpful to1 thankful Users |
12/30/2022 7:33 AM | |
Joined: 3/11/2019 Last visit: 4/30/2024 Posts: 1385 Rating: (246)
|
Hi,
do this with an empty project as already written, the firmware difference does not matter. Use the complete upload as new station including hardware + software. BUT: Uploading a project with V16 which was written in V15.1 will not work anyways. If the project currently on/in the CPU is written with V15.1, you will also need V15.1 for the upload. There is no other option. Please check out following FAQ. What options are available in STEP 7 (TIA Portal) for uploading when the project version in the CPU no longer matches the version on your PG/PC?regards sancruz |
Last edited by: sancruz at: 12/30/2022 07:34:24Feedback appreciated, please rate |
|
Follow us on