5/30/2024 11:32 AM | |
Joined: 11/9/2008 Last visit: 8/23/2024 Posts: 410 Rating: (6) |
Hi All, I need help tuning the temperature controller for the Steam valve. I am using FB41 as a PID block for the Steam control valve. I am facing a problem while tunning PID. Suppose theSet point is 120my temperature goes up to124 and downside 116. I have obeser the action of PID output whenPV goes above Set Point e.g 121 then PID starts taking actionsame for down side when PV goes down below Set Point the PID starts Taking action. I need PID to start taking action when PV starts reaching the Setpoint. Please help me whether I am missing something or need to use FB58 [ Temperature Controller ]. One more question Will FB58 work in S7-1500? or suggest the PID for the S7-1500 Controller? Waiting for your valuable reply. Regards, Yogendra
------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 05/31/2024 04:48:05New subject after splitting |
|
5/31/2024 4:48 AM | |
Joined: 6/19/2017 Last visit: 9/6/2024 Posts: 8175 Rating: (172) |
Closed cause question posted twice. The second thread with the subject PID for Temperature Controller Tuning Problem is published within the conference SIMATIC Technology. Jen_Moderator |
Follow us on