Industry Online Support
Technical Forum
7/27/2009 4:07 PM | |
Joined: 10/8/2008 Last visit: 5/22/2024 Posts: 43 Rating:
|
Hello, we want to communicate with a 315 PN as a slave and the master is a module from invensys (Foxboro) (M232) we are now using the wizard version 2 ID 31535566 and the trail programs. with the wizard we defined the master with the port 502 and de the IP adres. and the ID = W#16#1 For the PLC we only made the IP adres. Using the variable table we can see that there is a connection established, but there is no response or reaction of the busy or done bit. In the program we use the FB102 with the version 3.0, I know that th enew version 3.1 is already availeble, but in a lot aff threads there seams to be communication with programms version 3.0 Is it possible for the version 3.0 to communicate with a non siemens device Too simulate the master wenow use a mod_Rsim program, it is possible that this programm is notable to function like a master. What isgoing wrong in the programm. AttachmentModbus_p.zip (696 Downloads) |
7/31/2009 8:07 AM | |
Joined: 10/3/2008 Last visit: 5/22/2024 Posts: 957 Rating:
|
You're welcome. |
Follow us on