Industry Online Support
Technical Forum
11/2/2011 10:05 AM | |
Joined: 1/26/2011 Last visit: 8/11/2022 Posts: 243 Rating:
|
Hello charlesm, there are two different ways how to move the data from the camera to the PLC. The first way is to program a OPC Client (with C#or C++) for the Data exchange between the OPC Server. The second way is over Modbus TCP Communication. Here you can find information about this way: Cognex Connect http://www.cognex.com/ProductsServices/VisionSystems/default.aspx?id=1504 Modbus TCP Wizard http://support.automation.siemens.com/WW/view/en/31535566 S7 OpenModbus/TCP http://www.siemens.com/s7modbus I hope this information helps you. regards bigfoot |
11/2/2011 4:08 PM | |
Posts: 89 Rating:
|
Hello, |
Follow us on