3/21/2023 10:44 AM | |
Joined: 5/24/2016 Last visit: 4/18/2024 Posts: 315 Rating: (49)
|
Hello. This is an English forum, so please try and keep it in this Language :) Here is a translation
To answer your question is not so straight forward as it depends on the machine tool builder, and I guess you are refering to the T buttons. When calling the FB1 function block in Step 7 you can add what IO number you want to use for the MCP. I have most commenly seen Input I0.0 and Output Q0.0 used (this is due to the example from siemens being like this) I have added an attachment with the mapping of the MCP and the FB1 block so you can see what you are looking for. As an example. If FB1 has I0.0 in the input - The map shows that the T12 button is IB0+6 - Bit 4 - This would be I6.4 If FB1 has I100.0 in the input - The map shows agian that the T12 button is IB100+6 - Bit 4 - This would be I106.4 Best Regards Riddersholm AttachmentMCP mapping - Targatte.zip (247 Downloads) |
This contribution was helpful to1 thankful Users |
3/23/2023 8:34 AM | |
Joined: 11/14/2018 Last visit: 12/11/2023 Posts: 8 Rating: (0) |
Hello Riddersholm, thank you for your answer, it helped me a lot best regard targatte |
Follow us on