11/26/2022 11:00 AM | |
Joined: 3/30/2020 Last visit: 2/8/2023 Posts: 3089 Rating:
|
I have attempted this suggestion, using the built-in unzip of Windows 10. It worked. Attached is the project that ixo65 gave, but without the complication of the ZAP file. Reminder: This project means nothing if WinCC Comfort (or higher functionality) is not installed. Reading the user passwords from the project is also not possible. But making new passwords for the users will be possible.
AttachmentProject7_V13_SP1.zip (32 Downloads) |
Follow us on