5/28/2014 10:01 PM | |
Joined: 4/19/2008 Last visit: 9/3/2024 Posts: 1525 Rating: (159) |
Hello Tony Dean, Which SIMATIC NET PROFIBUS PC CP is compatible with which Microsoft Windows operating system? CP 5622 PCI EXPRESS X1-CARD FOR CONNECTING A PG OR PC WITH PCI EXPRESS-BUS TO PROFIBUS OR MPI CAN BE USED WITH 32BIT AND 64BIT OPERATING SYSTEMS |
Ammy |
|
5/28/2014 10:18 PM | |
Joined: 9/27/2006 Last visit: 9/27/2024 Posts: 12283 Rating: (2685) |
Hello Tony; Based on the following document, I would doubt that you can implement the DP-Bse Programming on a CP 5622: Readme file for the "SIMATIC NET PC Software V8.2.1" DVD with important information on the products https://support.automation.siemens.com/dnl/DA/DAzNzUxOQAA_75914383_Akt/Readme_V821.htm You will see in the first table provided in the document that the DP-Base Programming Software is described as a Hardnet product, whereas the CP 5622 is a Softnet processor, This would make them incompatible, they require different Simatic Net drivers. The only suggestion I can make is to open a Support Request so that you can ask Siemens Support directly if they have some suggestions, besides the purchase (or transfer from your existing system) of a CP 5613 in the new Rack PC. See the link ast the right of this page. Hope this helps, Daniel Chartier |
Follow us on