1/12/2022 4:24 PM | |
Joined: 11/6/2020 Last visit: 4/15/2024 Posts: 14 Rating: (3) |
I use DrawIO to make SVG drawings and just drag-and-drop the file into my screen. |
1/21/2023 5:22 PM | |
Joined: 6/26/2008 Last visit: 4/13/2024 Posts: 48 Rating: (5) |
Hi, WinCC uses its own variant of svg with the extension .svghmi. You can start by designing an svg with one of the tools mentioned above. This involves changing the header, inserting an hmi.self object which contains the an hmi:paramDef object which specifies the parameters that are used to make the svg dynamic. In the remainder of the file you can replace static attributes with hmi:bind ones. Some svg features are not available in svghmi. It can be helpful to look at some of the svghmi files that are in the library. You need to save your own svghmi files at <project directory>\UserFiles\SVGControls Some errors in svghmi files can cause TIA v17 to crash or runtime to open without a start screen. If that happens, delete your svghmi file(s) and remove the corresponding objects from your screens. Attachment109782045_WinCC_and_SVG_DOC_de.pdf (573 Downloads) |
This contribution was helpful to2 thankful Users |
Follow us on