12/29/2023 2:36 PM | |
Joined: 9/23/2005 Last visit: 1/14/2025 Posts: 4392 Rating: (1463)
|
Hi As from TIA V19, it is possible to assign dynamic values to the names of variables passed as an interface in the Faceplates call. This feature enables the “multiplex” faceplate interface dynamically in runtime and could be used as a similar feature as the tag prefix of WinCC Professional / WinCC V8. TIPs
“ Defines a tag name which is composed of static parts and tag references. The resulting tag name is determined in runtime by replacing the tag references with the current tag values. Tag references must be encapsulated by single quotation marks (‘). Examples: 1. ‘UnitTag’.’MotorTag’.Temperature 2. Section[‘SectionNumber’].Conveyor2.Speed “ Sample project (archived from TIA Portal as .zap19 and after that compacted in .zip format to be uploaded here) user= User, all password = Password1! AttachmentPrefix_20231229_1008.zip (872 Downloads) |
Denilson Pegaia |
|
This contribution was helpful to2 thankful Users |
1/2/2024 9:07 AM | |
Joined: 9/23/2005 Last visit: 1/14/2025 Posts: 4392 Rating: (1463)
|
Hi As from TIA V19, it is also possible to suspend the faceplate’s scripting processing when it isn’t visible. This improves the performance, especially for screens with many faceplates. TIPs:
Sample project (archived from TIA Portal as .zap19 and after that compacted in .zip format to be uploaded here) user= User, all password = Password1! Attachmentsuspendable_20231229_0837.zip (605 Downloads) |
Last edited by: Denilson Pegaia at: 01/02/2024 09:12:20Denilson Pegaia |
|
1/3/2024 9:23 AM | |
Joined: 9/23/2005 Last visit: 1/14/2025 Posts: 4392 Rating: (1463)
|
Hi As from TIA V19, it is also possible to suspend the faceplate’s scripting processing when it isn’t visible. This improves the performance, especially for screens with many faceplates. TIPs:
Sample project (archived from TIA Portal as .zap19 and after that compacted in .zip format to be uploaded here) user= User, all password = Password1! Attachmentsuspendable_20231229_0837.zip (558 Downloads) |
Denilson Pegaia |
|
1/5/2024 9:44 AM | |
Joined: 9/23/2005 Last visit: 1/14/2025 Posts: 4392 Rating: (1463)
|
Hi As from TIA V19, it is also possible to suspend the faceplate’s scripting processing when it isn’t visible. This improves the performance, especially for screens with many faceplates. TIPs:
Sample project (archived from TIA Portal as .zap19 and after that compacted in .zip format to be uploaded here) user= User, all password = Password1! Attachmentsuspendable_20231229_0837.zip (548 Downloads) |
Denilson Pegaia |
|
This contribution was helpful to1 thankful Users |
1/10/2024 9:47 AM | |
Joined: 9/23/2005 Last visit: 1/14/2025 Posts: 4392 Rating: (1463)
|
Hi As from TIA V19, it is possible to save text lists in the type library and use these type library text list objects in a Faceplate. TIP:
Sample project (archived from TIA Portal as .zap19 and after that compacted in .zip format to be uploaded here) user= User, all password = Password1! AttachmenttextList_20231229_1625.zip (489 Downloads) |
Denilson Pegaia |
|
Follow us on