工业业务领域支持中心
Technical Forum
5/20/2006 5:32 PM | |
Joined: 1/7/2006 Last visit: 11/17/2023 Posts: 2705 Rating:
|
Hi Ger, I believe that it have something to do with the simulated DOS-program, i have normally with STEP5 under Windows XP only that it is starting not that fast, but after that it works fine. In the Executability of COM Packages Under STEP5/ST V7.x is Windows XP not tested... http://support.automation.siemens.com/WW/view/en/9715828 Only STEP5 V7.2 is tested under Windows XP, COM GRAPH V2.33 is tested with S5 V7.2 http://support.automation.siemens.com/WW/view/en/6002243 I have seen a FAQ with some things to set up for STEP5 under Windows 2000, but i couldn't find it anymore... [:blush:] |
I hope that the answer will help, if you have still questions, don't hesitate to ask me. |
|
Follow us on