10/26/2021 8:12 PM | |
Posts: 257 Rating: (78)
|
Hello SIOS Forum Community, Our customers often use WinCC Flexible 2008 SP1/2/3 and have to move the engineering or runtime (RT) to a new computer with Windows 10 when changing the system, e.g. the hardware and the operating system. The problem here is that these versions are not released for Windows 10. As a solution, we recommend downloading and installing the TRIAL version of WinCC flexible 2008 SP5 (executable under Windows 10). After installing this software, only the existing licences for engineering or RT need to be transferred to the new computer using the Automation License Manager (ALM). SIMATIC WinCC Flexible 2008 TRIAL Download: https://support.industry.siemens.com/cs/ww/en/view/100777999 Important note: Please be sure to check the compatibility of the Windows 10 version with WinCC flexible 2008 SP5. This check can be easily carried out with the compatibility tool. Link compatibility tool: https://support.industry.siemens.com/kompatool/pages/main/index.jsf Best regards, SIMATIC International Technical Support Hub |
Follow us on