4/17/2023 7:36 AM | |
Joined: 7/5/2013 Last visit: 7/18/2024 Posts: 3107 Rating:
|
Hello Otavio, please see SIMATIC WinCC WinCC Engineering V16 – Programming reference. In the system manual you will find that there are differences between "VBScript for Windows" and "VBScript for Windows CE". Windows CE is the operating system of the panels and you have to check chapter 1.4 of the system manual. E.g. "FileCtl.File" instead of "Scripting.FileSystemObject", both with different control elements. From my point of view this section of the programming reference is the same for WinCC flexible and WinCC TIA. Regards, Frink |
Pi is exactly three! |
|
This contribution was helpful to
1 thankful Users |
4/17/2023 1:07 PM | |
Joined: 8/3/2009 Last visit: 8/6/2024 Posts: 13467 Rating:
|
Hello Otavio Gomes(Alph... Here are examples for WInCC flexible: PC RT/Simulation: https://support.industry.siemens.com/cs/ww/en/view/26106418 Panel WinCE: https://support.industry.siemens.com/cs/ww/en/view/26107211 differences: https://support.industry.siemens.com/cs/ww/en/view/13408815 Bye Murof |
If this Information really helps, you could use the Rate function |
|
This contribution was helpful to
1 thankful Users |
Follow us on