6/10/2023 4:41 PM | |
Joined: 1/12/2023 Last visit: 9/20/2023 Posts: 3 Rating:
|
Hello everyone A} Currently I am using IM 155-6PN (6ES7155-6AA01-0BN0) in a project. Is it ok if I use all 32 slots of IM155-6? Is a power supply(rack mounted) needed to drive that much I/O? Actually I am using two IM155-6 in the control panel as follows . 1) IM155-6 with :- 4CH,2A, DO:- 23 NOS. 2) IM155-6 with 4CH,2A, DO:- 29nos; 8CH, DI:- 1NO and 4CH, AI:-2 Nos. B} Combination of BA and ST card we can use against above IM 155-6 Please suggest any corrections required ------------------------------------------------------------------------------------------ |
Last edited by: Sahil08 at: 06/11/2023 06:12:58Last edited by: Jen_Moderator at: 06/21/2023 09:29:57New subject after splitting |
|
Follow us on