7/27/2023 3:58 PM | |
Joined: 12/1/2020 Last visit: 8/14/2023 Posts: 19 Rating:
|
Hi All I have a similar requirement. I have a 200ppr encoder and want to give a voltage 0-10v to a UV system to control intensity of the the UV light output. The encoder has a 200mm wheel so 5 x revolutions is 1 meter If we say the lines maximum running speed is 100m/min 0v would be off 1v would be 10% - 10m/min and so on with 10v been 100% Distance/Speed 100m/m Rotations p/m 500 Frequency approx. 1666.7 Hz What blocks can I use to measure the incoming pulse/frequency/speed and convert this to an analogue 0-10v output depending on the incoming signal? Sorry if this is very confusing Thanks in advance
------------------------------------------------------------------------------------------ |
Last edited by: AJB_Domino at: 07/27/2023 15:59:32Last edited by: Jen_Moderator at: 07/28/2023 08:31:09New subject after splitting |
|
7/27/2023 4:15 PM | |
Joined: 12/18/2014 Last visit: 6/20/2024 Posts: 33213 Rating:
|
Hello AJB_Domino, which LOGO! have you exactly? |
7/27/2023 5:59 PM | |
Joined: 12/18/2014 Last visit: 6/20/2024 Posts: 33213 Rating:
|
Maybe this helps you ...
AttachmentConversion_pulses_to_voltage_0BA8.Standard.zip (474 Downloads) |
8/4/2023 2:41 PM | |
Joined: 12/1/2020 Last visit: 8/14/2023 Posts: 19 Rating:
|
Sorry for the delay I have a 12/24rce Thanks Adam |
8/4/2023 2:54 PM | |
Joined: 12/18/2014 Last visit: 6/20/2024 Posts: 33213 Rating:
|
Okay, 12/24 RCE LOGO!s have fast inputs (I3-I6). |
Follow us on