12/21/2023 8:14 AM | |
Joined: 5/6/2010 Last visit: 6/27/2024 Posts: 1970 Rating:
|
Hello, there is no expansion module at the ET200SP. You need another IM with another IP-address. Otherwise you have a lot of sensors with M12, you can use the ET200AL. There is a module to connect directly to the ET200SP and so you expand your station. The module is the ET 200SP, Busadapter BA-Send BA1XFC (6ES7193-6AS00-0AA0). regards |
This contribution was helpful to
1 thankful Users |
Follow us on