2/21/2024 2:49 PM | |
Joined: 7/19/2022 Last visit: 6/13/2024 Posts: 364 Rating: (61) |
Hello agapit1988, I tell you: 1) I attach the download link for the 21-day trial version of TIA Portal with WinCC Comfort: SIMATIC STEP 7 inkl. Safety, S7-PLCSIM and WinCC V19 TRIAL Download 2) The connection to the PC is made through a normal Ethernet or PROFINET cable: SIMATIC HMI HMI devices Comfort Panels. Connecting the configuration PC 3) There are no default passwords. Only those that you configure in the project. But if you want, you can do a Reset to factory settings on the screen through Prosave as indicated in the document "Operating System Update" and "Reset to Factory Settings" with ProSave (Stand alone)" at the following link: How do you do a SIMATIC HMI operating system update (firmware update, OS update) on operator panels or perform a "Reset to factory settings"? You can download Prosave from here: Servicetool SIMATIC ProSave |
If this Information really helps, you could use the Rate function |
|
This contribution was helpful to1 thankful Users |
Follow us on