6/17/2015 3:30 PM | |
Posts: 160 Rating: (9) |
Are those bits in array or are defined independently? |
This contribution was helpful to1 thankful Users |
1/29/2016 1:14 PM | |
Joined: 7/24/2014 Last visit: 12/4/2023 Posts: 392 Rating: (66) |
Dear venkatesh Programming in plc can be done but i have another solution in which the C script will take care of the word bit edit. Here below attachment i am sharing please check it out . Smit Shah if helpfull then please rate Attachmentscript_sss.rar (951 Downloads) |
Thanks and Regards |
|
This contribution was helpful to1 thankful Users |
9/26/2018 11:17 AM | |
Posts: 1 Rating: (0) |
Helo SIr Can u please guide me how to convert bits into words , i have 16 bit BOOL values that i have to convert into a word |
Follow us on