4/20/2021 1:30 PM | |
Joined: 8/13/2019 Last visit: 1/18/2023 Posts: 2 Rating: (1) |
Hi, If I understand you correctly what you want: For the Webserver you have to set a Username and Password in the WInCC Internet Settings -> "Webserver" -> User Administration (HMI control panel). Define a new User and set the Authorisations. Hope this helps. P.S. create also button on the HMI which will open you control panel (then you don't need any person on the site, you can do everything remote). Regards AttachmentUser.docx (800 Downloads) |
Last edited by: AutoGen_9656606 at: 04/20/2021 13:34:08 |
|
This contribution was helpful to2 thankful Users |
7/15/2024 10:25 AM | |
Joined: 4/7/2009 Last visit: 7/15/2024 Posts: 9 Rating: (0) |
it could be a little late to answer, anyway, to get to the Wincc Internet settings: 1- unplug and re-Plug again the 24vdc power supply of the HMI 2 -press at the Settings 3-you can see the the Wincc Internet settings. continue as already decribed from AutoGen_9656606 AttachmentWincc Internet setting.docx (189 Downloads) |
Follow us on