9/16/2024 7:01 PM | |
Joined: 9/18/2012 Last visit: 9/16/2024 Posts: 2 Rating: (0) |
The BDA devices have been obsolete for a long time. They can no longer be supported because of security issues with the embedded Java that is contained in the BDA. I can honestly not recall whether Powerconfig supported the BDA. We have had good success both with the TD400 and using a COM16 or COM35 module as an interface between the ETU and Powerconfig. The attached file shows how to use a COM16 but using a COM35 works exactly the same way. AttachmentCOM16 as a Parameter Setting Interface V5.pdf (119 Downloads) |
Follow us on