11/30/2021 3:44 PM | |
Joined: 10/19/2021 Last visit: 10/24/2024 Posts: 2 Rating: (0) |
Hello, i'm using TP1500 comfort with a S7 1500 and in i'm having the same problem. the error description says: "The address of the tag '..' cannot be determined. Specify the address or re-establish the PLC connection with the connection name: 'HMI_Connection_2'.,,,3:20:13 PM. I've already checked and the IP address i correct and the plc. thx. Best regard Christian. ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 12/01/2021 08:30:19New subject after splitting |
|
2/2/2023 5:28 AM | |
Joined: 8/2/2022 Last visit: 2/17/2023 Posts: 1 Rating: (0) |
I was able to resolve this issue by doing a Compile -> Software (rebuild all) on the PLC and then the same on the HMI. |
Follow us on