9/11/2024 3:52 PM | |
Joined: 3/19/2019 Last visit: 9/23/2024 Posts: 104 Rating: (0) |
Dear bg2492, Can you help me to configure S7-400H Redundant PLC conncetion with TIA WinCC Professional V19?
------------------------------------------------------------------------------------------ |
Last edited by: Wit_Moderator at: 09/12/2024 11:58:23New subject after splitting "If you want the answer - ask the question" |
|
9/13/2024 2:33 PM | |
Joined: 2/17/2020 Last visit: 10/9/2024 Posts: 1079 Rating: (192) |
Hi, In principle the "Software redundancy" option is not released for WinCC Professional and S7-400H combination. However, I believe that it should be possible to "reuse" the example for "Software redundancy" from classic WinCC V7.X, which means that the changeover of the connection could also be used in WinCC Professional after some small adjustments. WinCC V7.5 SP2: Configuration and communication > Software redundancy If someone has managed to do this and would like to share it, that would be very helpful. |
A rating will be well appreciated. |
|
Follow us on