工业业务领域支持中心
Technical Forum
6/1/2010 1:07 AM | |
Posts: 2661 Rating: (279) |
Hi th0ny_15, Have you tried uninstalling and re-installing the ALM? Regards |
6/1/2010 4:11 AM | |
Posts: 2661 Rating: (279) |
Please have a look at the following: How do you uninstall SP3 of Microsoft Windows XP? |
6/1/2010 9:09 AM | |
Joined: 3/21/2006 Last visit: 7/26/2024 Posts: 10228 Rating: (1181) |
Hello, From one side, of course you should install ALM into compatible area. Also to keep it up to date is useful - ALMv40SP5.zip .Then should install there licenses which you have propely - How do you install, uninstall and upgrade authorizations? .If you have troubles with ALM and licenses contact with Siemens Hotline at - How can you recover defective licenses and authorizations? Simple and fast. Best regards, Hristo Mihalev |
6/1/2010 10:33 AM | |
Joined: 11/15/2006 Last visit: 5/7/2021 Posts: 1319 Rating: (172) |
Switch the view from "search results" to "license keys" once. Does it change anything? Is there an error message upon start of Windows or in Windows Eventlog? Something like "cryptographic provider initialization failed"? If so and there is just an red "X" in ALM visible, try following MS solution: http://support.microsoft.com/kb/246183/de |
Have Fun! |
|
Follow us on