工业业务领域支持中心
Technical Forum
11/18/2011 7:54 AM | |
Joined: 8/31/2010 Last visit: 11/6/2024 Posts: 1523 Rating: (229) |
Hello William B., Yes it is possible in panels. It isknown as GMP (Good Manufacturing Practice)Go through this for having the overview- SIMATIC WinCC Audit (TIA Portal) You can also make notes when making changes in the parameters. Find tech details from here.- Following GMP with Audit |
Like it? Rate it! |
|
This contribution was helpful to1 thankful Users |
11/18/2011 1:13 PM | |
Posts: 3037 Rating: (192)
|
Hello, You can use a TP277 or higher for Audit. You have no possibilities where you can save user actions at basic panels. Tweety |
11/18/2011 1:44 PM | |
Joined: 8/31/2010 Last visit: 11/6/2024 Posts: 1523 Rating: (229) |
Hello William B., In addition all of the SIMATIC HMI Comfort Panels support archives in turn Audit (starting from 4" display size ) - Delivery Release: SIMATIC HMI Comfort Panels |
Like it? Rate it! |
|
Follow us on