工业业务领域支持中心
Technical Forum
2/5/2007 7:47 PM | |
Posts: 42 Rating:
|
I'm trying to activate PROFIBUS communication betwen PLC and danfoss drive (VLT 6000-DPV1) and I have some problems ....(I use danfoss GSD file for VLT 6000, danfoss communicaton blocks (from PCA channel danfoss write /read project from danfoss page), PPO type 1, word consinstent) My questions and problems are next: 1) [:cry:]Can I use this blocks from danfos project (in the project they are used with FC 300) ? 2) [:cry:]The next problem is that I can change only the first parameter in write/read parameter block and not the others ..... 3) [:cry:]How could I stop and start the drive from PLC withoute cousing PLC problems (SF,BF) can I use OB 82, 86,100 and how 4)[:(] Is there any other example of Siemens DANFOSS VLT 6000 or any other easier way of communicating betwen PLC and danfoss drive. Any informationor example ismore then helpful[:cry:] This is the danfoss project for FC 300... (my is based on itwith few modifications for VLT 6000) AttachmentPCA_BL~1.ZIP (1005 Downloads) |
Follow us on