8/19/2018 9:17 AM | |
Joined: 9/9/2015 Last visit: 9/29/2024 Posts: 42 Rating: (0) |
Hi, We had a proTool HMI application running on a PC 670. But now we have substitute the PC 670 with a FI45. The application runs well but now the S1-S12 Keys are not working anymore. Should I install any special driver to make these keys work? Right now the PC/AT Enhanced PS/2 keyboard(101/102Keys is installed on the driver section of keyboards. PS: 2 pictures are upload on the below links [snip] AttachmentImages.zip (216 Downloads) |
Last edited by: Jen_Moderator at: 8/20/2018 1:09:51 PMRemoved links and added files as an attachment. |
|
8/19/2018 10:11 AM | |
Joined: 9/9/2015 Last visit: 9/29/2024 Posts: 42 Rating: (0) |
I find this keytools to install. But the help file in the following zip file refers to a "TACOUSB_W2K.EXE" which I can't find in the zip file. any help? |
Last edited by: Jen_Moderator at: 8/20/2018 1:11:06 PMOptimized link. |
|
8/19/2018 10:22 AM | |
Joined: 9/9/2015 Last visit: 9/29/2024 Posts: 42 Rating: (0) |
I've also find this link . But it seems that the file has been deleted from Siemens website. Where can I find this file? |
Follow us on