工业业务领域支持中心
Technical Forum
11/5/2008 9:01 AM | |
Joined: 4/24/2006 Last visit: 11/14/2024 Posts: 8768 Rating: (1171) |
Dear Paresh, I believe it has to do with Consistency Have you programmed Total consistency, then you should use SFC14 and SFC15 to communicate with slave. See following link: http://support.automation.siemens.com/WW/view/en/8751062 Here is manual, where you can find more information about SFC14 and SFC15: http://support.automation.siemens.com/WW/view/en/1214574 Best regards, Wizard |
11/18/2008 8:16 AM | |
Posts: 116 Rating: (1) |
Hi Wizard, Can you explain me the word Consistency in referece with Profibus as I always has confusion with it. Thanks Regards Paresh |
11/18/2008 10:35 AM | |
Posts: 116 Rating: (1) |
Hi Wizard, Thanks for the information. The word "Consistency" is clear to me now. Regards Paresh |
11/18/2008 11:14 AM | |
Joined: 4/24/2006 Last visit: 11/14/2024 Posts: 8768 Rating: (1171) |
You are welcome Best regards, Wizard |
Follow us on