工业业务领域支持中心
Technical Forum
8/11/2010 3:03 PM | |
Joined: 7/28/2010 Last visit: 8/31/2024 Posts: 184 Rating: (11) |
Peva, You should be able to click, hold and drag it to centre of the screen. Regards, Behnam www.sigmaprocess.ca |
8/12/2010 7:55 AM | |
Posts: 38 Rating: (0) |
Well, the problem is, that to click+hold+draw, one must do it on window title, or at least border. And my problem is, that the window title in my case is just desperatedly off screen, so I can't click it, and the border on this window apparently doesn't exist. I see just a couple of left side buttons and when I click + draw on any of them, nothing happens (just the button is pressed). I guess this is the standard Windows behavior. Regards, Petr |
8/20/2010 2:34 PM | |
Posts: 26 Rating: (0) |
Whydon'tyou try this program. It can move the keyboard position to the mouse position by pressing the mouse wheel button. Free trial available here :http://www.download32.com/on-screen-keyboard-magic-i32848.html
|
8/23/2010 10:18 AM | |
Posts: 38 Rating: (0) |
Are you sure it will work with the Siemens keyboard? I tried it on my PC and it looks it is developped only for the standard Windows keyboard. Anyway, thanks for the hint. Petr |
2/1/2011 10:51 AM | |
Posts: 7 Rating: (0) |
Hello all, Any news on this matter? I got the same problem with my MP377 "15 Multi panel. I cant find anything about it anywhere. Only this posts above shows the same problem as I do. Does anyone knows how to fix it? (That virtual keyboard AL81@lit doenst work) Thanx! Johnny. |
Follow us on