1/31/2023 8:59 PM | |
Joined: 6/9/2022 Last visit: 8/9/2023 Posts: 6 Rating: (0) |
Hola ChristophD. Tengo un problema con una CPU d435-2, esta misma al principio se queda en stop, con los leds ready=on, stop=on y sf=on.Para que seas consciente.La tarjeta CF estaba dañada, la reemplacé por una con la versión más actual, realicé todos los cambios de hardware y luego la descarga.Después de todo, la unidad no entra en modo de ejecución.Adjunto una imagen del buffer.Agradeceré cualquier ayuda. ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 02/06/2023 10:58:58New subject after splitting |
|
2/2/2023 9:03 AM | |
Joined: 8/21/2014 Last visit: 9/12/2024 Posts: 1033 Rating: (14) |
Please try to discuss your question in English language. This is an international community and we try to focus on one language. Posting in English will help you to get more response to your question. This is the translation of your question:
|
My Forum is the place to personalize your profile, |
|
2/6/2023 5:22 AM | |
Joined: 5/12/2006 Last visit: 9/3/2024 Posts: 22352 Rating: (3008)
|
see the other topic from you |
This contribution was helpful to1 thankful Users |
2/6/2023 11:02 AM | |
Joined: 6/19/2017 Last visit: 9/6/2024 Posts: 8175 Rating: (171) |
Closed cause question posted twice. The second thread with the subject Simotion D435-2 in stop is published within the conference Motion Control System SIMOTION. Best regards, |
Follow us on