4/24/2023 2:13 PM | |
Joined: 1/6/2021 Last visit: 9/16/2024 Posts: 10 Rating: (0) |
Hello, i`m busy with the IOT2050 and in total i have to say, i like it. At the moment i`m stuck because of a Modbus TCP problem, maybe someone can help me. I try to setup a Modbus TCP server. Writing from the Laptop to the server is after a few hours working. For example: Registers 0-10 is only for writing (Laptop-Client writes to the IOT2050) BTW: i`m open for any training suggestions Thanks for helping, Attachmentflows.txt (503 Downloads) |
Follow us on