9/27/2023 9:15 AM | |
Joined: 9/4/2023 Last visit: 4/9/2024 Posts: 4 Rating: (0) |
since radusti333 is no longer working on this subject for his graduation assignment i have taken over I will answer. while the mcp251x driver is indeed included in the full kernel it is not in the siemens example inmages nor does trying to include it in the build process work using the ONFIG_CAN_MCP251X=y option in the iot2050_defconfig_extra.cfg file. it is possible to include the peak_usb can driver using CONFIG_CAN_PEAK_USB=y but not the pci variant using CONFIG_CAN_PEAK_PCIEFD=y kind regards Max van Eck ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 09/27/2023 11:24:47New subject after splitting |
|
Follow us on