3/19/2024 9:41 AM | |
Joined: 3/11/2019 Last visit: 8/20/2024 Posts: 1555 Rating: (281)
|
Hi, which one exactly, because there are different ones with different interfaces: 1. V680S-HMD66-EIP In this case it's an "EtherNet/IP" device and you can use following library EtherNet/IP Scanner – Connecting third party I/O’s using EtherNet/IP2. V680S-HMD66-PNT In this case the device uses PROFINET. The connection is like for any other PROFINET io-device on the market.
regards sancruz
|
Last edited by: sancruz at: 03/19/2024 09:43:08Last edited by: sancruz at: 03/19/2024 10:34:40Feedback appreciated, please rate |
|
Follow us on