3/15/2024 12:35 PM | |
Joined: 6/15/2023 Last visit: 3/22/2024 Posts: 11 Rating: (0) |
Hi, I'm having difficulty making an HTTPS GET request to an API created on Insights Hub (gateway.eu1.mindsphere.io...) on the PLC S7 1200. It always returns the error 'No valid certification authority found.' This error is specifically occurring with these APIs. I tested with an API created on GitHub, and it worked perfectly. In both cases, I obtained the certificate authority in the same way. I have no idea why the certificate isn't working. Note that this Insights Hub API works fine in Postman and Node-RED. AttachmentError API Mindsphere.pdf (109 Downloads) |
Follow us on