4/10/2024 11:50 AM | |
Joined: 5/21/2013 Last visit: 9/26/2024 Posts: 8 Rating: (0) |
Hello, I'm trying to get a CP 1243-7 to send alarm SMS messages to mobile devices. The problem is that when I use CP 1242-7 all work great but with CP 1243-7, FB3 - BroadcastSms has error state 16#0001_809A It's state of TSEND_C and means: The CONNECT parameter points to a field that does not correspond to the length of the connection description. But why with CP 1242-7 everything is ok and CP 1243-7 is the problem? Any idea? Thank you. ------------------------------------------------------------------------------------------ |
Last edited by: tomas.belko at: 04/10/2024 11:50:21Last edited by: tomas.belko at: 04/10/2024 13:08:38Last edited by: Jen_Moderator at: 04/11/2024 06:03:52New subject after splitting |
|
Follow us on